STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

FreeRTOS Version

Thank you for helping.environment:Board: STM32F769I-DISCOTouchGFX: Ver4.15.0Is it possible to set the version of FreeRTOS (osCMSIS) to 1?If it is 2, other (LwIP) does not work well, so I would like to try it with 1.Thank you.

Ebun.1 by Senior
  • 2111 Views
  • 6 replies
  • 0 kudos

Issue with migrated project between 4.13 to 4.15

My result for use CubeIDE versions is strange. Every version have deep troubles.One my project i handle over versions and end with TouchGFX 4.13 in CubeIDE 1.3.1 and MX 5.6.1, with perfectly working code.Half year after i use second PC and install n...

MM..1 by Chief III
  • 710 Views
  • 0 replies
  • 0 kudos

Problem with Updating Frame buffer of LTDC

When I update the LTDC Frame buffer, showing the display has problem.I use DMA2D and FBAdress located in external SDRAM.I write in pixels as follows (e.g. 1000 Pixels):__IO uint32_t* Address = (uint32_t*) 0xC0000000; __IO uint32_t Data = 255;while(1)...

0693W000005Cjp3QAC.jpg
Slh by Senior
  • 2004 Views
  • 4 replies
  • 0 kudos

Migrating from TouchGFX 4.13 project to 4.15 prevents original user added imagery that was in (_designer) folder from being assignable to controls in 4.15 Designer

Good Morning,I have a project created in TouchGFX 4.13 with user images that were automatically placed into a folder named _designer. Although 4.15 can display those images in the Images tab, they are not assignable to any newly added controls. They ...

HGran.1 by Associate II
  • 1368 Views
  • 2 replies
  • 0 kudos