cancel
Showing results for 
Search instead for 
Did you mean: 

Can I get TouchGFX + TruyHandsfree demo application source code ?

Shree
Associate II

Hi @Martin KJELDSEN​ ,

1) Is it possible to share the source code for TouchGFX TrulyHandsfree demo ?

https://youtu.be/B8_2XtEK4wk?list=UUPmAQbY9KbHqdQ_GwUGg1bA

2) I am planning to buy STM32F469 Discovery kit for Alexa implementation. Does ST provide Audio codec, Mic etc drivers with this kit ?

Regards,

shree

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Alexandre RENOUX
Principal

Hello,

1) For the TrulyHandsFree demo, I'll check if it's possible to share the code and will come back to you.

2) Regarding Audio codec, Mic, drivers, please ask in the corresponding topic as it is not directly related to TouchGFX.

/Alexandre

Shree
Associate II

Hi @Alexandre RENOUX​ ,

Did you check if it is possible to share the sensory demo code ?

Regards,

Shree

Alexandre RENOUX
Principal

Hello,

For the demo shown on the video, most of the graphics are available trough TouchGFX Demo 1 and 2 in TouchGFX Designer. The demo you see on the video is an old one involving 3rd party code.

As for the voice recognition, this cannot be share.

Very sorry for the late answer.

/Alexandre