STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Touch Gfx using LTDC 2 layers

Hello I see on this link that Touch Gfx can only use a single layer from the LTDC.https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-ltdc-parallel-rgb Is there some way of using the two LTDC's layers ?,May be i...

Failed to simulate with STM32H750ZBT6 platform

I build a LCD driver board with STM32H750ZBT6  ,then i want to use built-in LTDC driver and SDRAM to run 480*270*16 TFT LCD panel , but touchGFX list following wrong message, where reason from ?        Generate CodeGenerateDoneGenerate Assetsmake -f ...

miker by Associate III
  • 534 Views
  • 1 replies
  • 0 kudos

Resolved! Simulate HW buttons in Simulator

Hi.We have an application with a touch screen and 4 physical buttons. We have designed a demonstration GIU in TouchGFX, but to allow the simulator to handle presses on the hardware buttons, we have added the hardware buttons on the display. Consequen...

Resolved! Single function to redirect to certain view

I'm having a Model that receives data from the backend. I need that, according to the data received, independently of what view you're in, the presenter of the view executes a function that goes to a specific view. For instance, I'm receiving 1 in th...

nico23 by Senior III
  • 540 Views
  • 4 replies
  • 0 kudos