User Activity

Good morning,I'm trying to generate code for a project made for a 7-inch Riverdi display (RVT79HSSNWC00-B).When I run "Generate Code" on TuochGFX it gives me the following error:"Generate CodeGenerateWrote generated/simulator/src/mainBase.cppDoneGene...
Good morning,we are working on a project using a 5 inch display (RVT50HQSNWC01-B) in the TouchGFX Designer environment. Simulation, code generation and code download to the MCU works.Problems arise when moving to STM32CubeIDE. In this environment, ca...
Good morning,I'm working on a graphics project on a 7 inch Riverdi display (RVT70HSSNWC00-B). I added a screen containing a video but I couldn't play it so I deleted the screen and ran the Run Simulator but it gives me this error:====================...
Good morning,we are trying to program a RVA15MD + NUCLEO-C071RB display. When loading the TouchGFX Demo 4 the programming is not successful (see errors in the attachment). While with the TouchGFX Demo 8 everything loads correctly and the demo works.C...