STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX server problem ?

Bonjour,Since this morning, I can't create touchGFX projects with my card anymore.I have this wonderful error message.My internet connection has no problems.I reinstalled touchgfx but still the same problem.

SGROU.1 by Associate III
  • 2584 Views
  • 3 replies
  • 0 kudos

stm32f769 LTDC + DSI only 1 frame then fadeout

I'm trying to run up a display with an ILI9806E controller but although I get encouraging flickers I only seem to get a single frame and then the display fades out.I've tried turning on the pattern generator with HAL_DSI_PatternGeneratorStart(), sam...

Resolved! LCD_CLK is not output from the microcomputer

Thank you for helping.environment:STM32CubeIDE Ver1.5.0TouchGFX Ver4.15.0Board: CustomMCU: STM32F769BIOutputs RGB parallel signals from the MCU.I want to output a 65MHz LCD_CLK, but the LCD_CLK signal is not output.Why?The transmitter is 25MHz and Sy...

Mna.1 by Associate II
  • 1891 Views
  • 3 replies
  • 0 kudos

Using SDRAM as ExtFlashSection for TouchGFX

Hello!I successfully created a user interface on an STM32F469I-DISCO which looks rather neat.However, with only a few icons it uses, the memory is already about 80% full. That's why I tried to use the embedded SDRAM to store the data required for the...

0693W000007DcNbQAK.jpg 0693W000007DcNMQA0.jpg
NKieg.1 by Associate III
  • 3921 Views
  • 6 replies
  • 0 kudos