STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! problem with dynamic graph

Hi, my problem is that when I use the dynamic graph, when it ends on the X axis, but unfortunately the X value increases How can I solve this problem and start the X axis again from scratch?

mbagh.1 by Senior
  • 1413 Views
  • 1 replies
  • 0 kudos

Resolved! How to make Fixed X-Label axis

I need to make application of pressure measurement across time by using dynamic graph feature. The X axis is time from 0 - 10 s. But as times go by beyond 10s, I want the X axis label remain as 0...10s instead of incremented for every data point adde...

BParh.1 by Senior III
  • 4257 Views
  • 9 replies
  • 0 kudos

Is it possible to drive a TouchGFX Application without actually having to touch or press a button on the display?

I have developed a device able to measure acceleration, so I essentialy have a GUI with a "start", "stop" buttons and also a text buffer showing the result of the last measurement.When I press the start button, a measurment starts and it keeps going ...

Ajudi.1 by Associate II
  • 1689 Views
  • 2 replies
  • 0 kudos

Touchgfx 4.16.1 on stm32h735 demo board work with Text and Font in internal flash but not with text and font in External flash. The images assets in external flash have never problem. Why?

My application demo is very simpe.I'm started with Cube MX 6.2.0 and the last stm32H7 Hal library available.I'm started with eval kit configuration pinout and I work with the STM32H735IGK6 eval kit.I have created a very simple application TouchGFX De...

RGenn.1 by Associate II
  • 1768 Views
  • 0 replies
  • 0 kudos

Resolved! problem with handleDragEvent

Hello, when I use handleDragEvent and handleClickEvent, widgets such as buttons and sliders that need to be clicked and dragged no longer work. How can I solve this problem?

mbagh.1 by Senior
  • 1826 Views
  • 2 replies
  • 0 kudos

How do I set the Model::Tick() cycle in TouchGFX?

There is a Model::tick() timer function in TouchGFX.I wonder if it is possible to set the calling period of this function.In my program now it is repeated every 0.285msec. I want to change this to be called every 15msec, so please give me advice on w...

PKunK.1 by Associate III
  • 6144 Views
  • 3 replies
  • 0 kudos

How to transition screen, without the designer

Hi,I have a screen that no other screen would transition to it with the help of interactions in the designer,I know I can transition to other screens with the help of this functionstatic_cast<FrontendApplication*>(Application::getInstance())->goto...

freertos and uart

I am trying to capture UART message once a button is pressed. I have implemented the functions to do that and while debugging i see the steps required to do that.However, when the UART communication happen, i get strange messages (check photo)Note: i...

BHure.1 by Associate III
  • 5305 Views
  • 8 replies
  • 0 kudos