STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Button vs. Clickable Icon

In terms of memory, performance, etc., is it preferable to implement a button or clickable icon? I assume that since a button is made of two images that a clickable icon is marginally more efficient. In my specific application, due to some constrai...

CPaye.1 by Associate III
  • 2319 Views
  • 2 replies
  • 0 kudos

Resolved! Using TouchGFX with STM32L476

Hi all,I want to use TouchGFX to manage a simple display with STM32L476. I generate the code with cubeMX and TouchGFX 4.16, but when I try to compile it a lot of errors comes up!There is any tutorial or guide on how setup touchGFX with this microcont...

MGiam.1 by Associate II
  • 1392 Views
  • 2 replies
  • 0 kudos

STM32F746G-DISCO, GFX, STM32CubeIDE

HiUse the buttons to set the sec and min. Use the START button to switch to ScreenCurrent. Press the STOP button to go to the ScreenSet. After switching to ScreenSet, I want sec and min to be automatically reset. How to set it up? greetingsAndrzej

Framebuffer in internal ram + CMSIS OS

Hi, I configured LTDC and TouchGFX properly without using os,I created internal framebuffer and linked it with this code:__attribute__ ((section(".TouchGFX_Framebuffer"), used))uint32_t framebuffer[400*200];However this is not working if I try using ...

AFire.1 by Associate II
  • 1114 Views
  • 1 replies
  • 0 kudos

Resolved! ScrollList can only host 6 items?

version: touchGFX Designer 4.16.1I generated a ScrollList to contain 8 itemsIn the .touchGFX project (attached) I can see the expected lines"Type": "ScrollList", "PaddingBefore": 0, "PaddingAfter": 0, "Snapping": false, "IsHorizontal": false, "IsCirc...

RReta.1 by Associate III
  • 1400 Views
  • 2 replies
  • 0 kudos

consistent camelCase usage

Repro steps (using TouchGFX Designer 4.16.1):Create a custom container class with a solid box background, named `background`Renamed a custom container class from `background` to `Background`This results in gui_generated base files of `backgroundBase....

RReta.1 by Associate III
  • 1019 Views
  • 2 replies
  • 0 kudos