STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Error: failed to download Segment[0]

So I have a STM32F769I-DISC0 board, and I am trying to write a binary file to it. Originally I was trying to write a binary file that was generated by the touchGFX Designer tool, but now I am simply trying to get the touchGFX example program for this...

CBurk.2 by Associate II
  • 2638 Views
  • 2 replies
  • 2 kudos

Resolved! Double buffer, one buffer is not updated

I have an application developed using touchGfx 4.13 where we are using a double buffer and it works fine. I have now migrated to touchGfx 4.17 but it seems like the double buffer is not working as expected. When I change from a longer text to a short...

LRose.3 by Associate II
  • 4046 Views
  • 7 replies
  • 0 kudos

Resolved! Is DCMI DMA on STM32H743 request 74 or 75?

according to https://www.st.com/resource/en/application_note/dm00373474-digital-camera-interface-dcmi-on-stm32-mcus-stmicroelectronics.pdf sec 4.4.3, it says request 74. But according to the reference manual https://www.st.com/resource/en/reference_m...

LKan.1 by Associate II
  • 2027 Views
  • 3 replies
  • 0 kudos

Resolved! Float wildcard precision limited to 6 digits ?

Hi,I try to display a float with a precision of 9 number after the digit. My wildcard buffer size is set to 20.Unicode::snprintfFloat(textArea1Buffer, TEXTAREA1_SIZE, "%.9f", 0.123456789f);   textArea1.invalidate();My output when running the simulato...

[Touch GFX] stm32f446 + spi-lcd(320x170). how to setup?

Dear specialist,I have to apply spi-lcd(with st7789v driver ic, 320x170) on our own ckt using stm32f446ve.Originally we've used STemWin lib with fsmc parallel i/f lcd(320x240), but this time we had to change due to lcd delivery problem. this time I ...

Tiel by Associate II
  • 859 Views
  • 0 replies
  • 0 kudos

Screen jitters with animation

Hello,I'm currently developing a project using Touchgfx on a custom board with a STM32F469II, external RAM/FLASH, SD card and a 1024x600 screen.I've recently come across an issue when performing any animation (slide screen transition, scrollable cont...

TDele.1 by Associate III
  • 6857 Views
  • 15 replies
  • 1 kudos