2021-09-27 4:35 PM
according to https://www.st.com/resource/en/application_note/dm00373474-digital-camera-interface-dcmi-on-stm32-mcus-stmicroelectronics.pdf sec 4.4.3, it says request 74. But according to the reference manual https://www.st.com/resource/en/reference_manual/dm00314099-stm32h742-stm32h743-753-and-stm32h750-value-line-advanced-arm-based-32-bit-mcus-stmicroelectronics.pdf Table 121, it says request 75.
Thanks
Solved! Go to Solution.
2021-09-28 2:21 AM
Hello @LKan.1 ,
The correct value for the DMA request MUX input for DCMI is 75.
I raised the request internally to correct the AN5020.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
2021-09-27 5:03 PM
How hard would it be to just see which one works?
2021-09-27 5:12 PM
Not very in my estimation, I'd go with the RM, odds of that are way better than 50/50
STM32Cube_FW_H7_V1.8.0\Drivers\STM32H7xx_HAL_Driver\Inc\stm32h7xx_hal_dma.h
#define DMA_REQUEST_I2C3_TX 74U /*!< DMAMUX1 I2C3 TX request */
#if defined (PSSI)
#define DMA_REQUEST_DCMI_PSSI 75U /*!< DMAMUX1 DCMI/PSSI request */
#define DMA_REQUEST_DCMI DMA_REQUEST_DCMI_PSSI /* Legacy define */
#else
#define DMA_REQUEST_DCMI 75U /*!< DMAMUX1 DCMI request */
#endif /* PSSI */
#define DMA_REQUEST_CRYP_IN 76U /*!< DMAMUX1 CRYP IN request */
#define DMA_REQUEST_CRYP_OUT 77U /*!< DMAMUX1 CRYP OUT request */
2021-09-28 2:21 AM
Hello @LKan.1 ,
The correct value for the DMA request MUX input for DCMI is 75.
I raised the request internally to correct the AN5020.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.