Skip to main content
DragonSal
Associate II
September 23, 2021
Question

Looking for Uctronics U6111 driver for STM32ST769

  • September 23, 2021
  • 0 replies
  • 483 views

Due to mechanical restrictions I'm being asked to implement an Uctronics U6111 display board with SPI interface. I've found the driver for for the display being used with Raspberry Pi (it's intended use) on github, but it appears to be a set of binary files, so I can't just convert it over.

I currently have it set up through the Arduino ports on the STM32F769I-DISCO and when power is enabled the display turns on and displays Uctronics. All this does is prove that the power cabling is correct. My next step is to import the driver, but I cannot find it anywhere.

I understand that using a Raspberry Pi display through the Arduino port of an STM32F7 board is not optimal, but this is being done to avoid retooling costs. Any help or suggestions would be appreciated.

This topic has been closed for replies.