STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Possible to communicate with TFT LCD panel driver registers (ILI6480BQ) over LTDC peripheral? Trying to rotate/orient display.

I'm using the LTDC peripheral to interface with a TFT LCD. It works great. Now I'm interested in rotating/orienting the display by 90 degrees. I have a couple approaches in mind - Doing some pointer gymnastics into the frame buffer that basically wri...

RMora.4 by Associate III
  • 2428 Views
  • 2 replies
  • 0 kudos

ID in bitmapdatabase.hpp

Hi,I would like to know if it is possible to 'freeze' the bitmap ID from build to build?I.e. give myself an ID...It is for a remote display with picto-button type, but the customer request is that he wants now a remote with a dynamic keypad. The butt...

PCu1 by Senior
  • 1925 Views
  • 2 replies
  • 0 kudos

Hello I have recently started working with touchgfx for migration of a project from F7 to H7 and touchgfx migration from 4.13 to 4.20. I have compiled the code as one of our project but the LCD goes white everytime I flash the code.

I am using a custom layout for the flash. A lot of the code is proprietay so I can share some parts of the code not the entire zip. Please understand. Can someone reply with any pointers that where should I look for such an issue ? I can share limite...

rohan_m by Senior
  • 1807 Views
  • 4 replies
  • 0 kudos