STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

slow gauge

I am using a custom gauge, but the movement of the needle is always not very smooth.is there any way to improve this?

DDi S.1 by Associate III
  • 5842 Views
  • 9 replies
  • 0 kudos

Resolved! Buttons/Box with rounded corner

HiI have the situation, that on one screen several buttons with only one color and rounded corners has to be placed. (see screenshot) But the corners are different on every button.The easiest way would be to generate two images (for released/pressed ...

Marco.R by Senior
  • 6700 Views
  • 7 replies
  • 1 kudos

some basic questions on charting, etc

I can make an application and load it into the IDE. I'm very familiar with programming the STM32s. I created a simple app that creates a dynamic chart. I can see where the dummy data is loaded into the chart in the base code. I have a few questions ...

LCD 1024x600, LTDC screen tearing using STM32H725

Hello everyone,Because I haven't found anything similar, I would like to ask you about my issue. The problem is screen tearing on the LCD with 1024x600 screen resolution. I'm using LTDC with RGB888 interface and RGB565 color format, so I have 16 bpp ...

0693W00000WIC2hQAH.png

TouchGfx modifies FMC SRAM lines

Hello, I'm using a STM32L4S9 with TouchGFX and an external SRAM on my custom board with cubeMX. However, I've found that after initialising the FMC lines, MX_TouchGFX_Init modifies the configuration of SRAM_D0 and SRAM_D1 on GPIOD, so that they can't...

AHugh.3 by Associate II
  • 2226 Views
  • 4 replies
  • 0 kudos

Touch Controller Board Reference

Hi,I'm currently working on the STM32H753I-EVAL02 with the 5.7" parallel RGB 24 screen.Now, I would like to buy a bigger screen with higher resolution (e.g. 7/8" - 1024*600). With this configuration, it's recommended to use LVDS rather than parallel ...

TLaur.3 by Associate II
  • 890 Views
  • 0 replies
  • 0 kudos