STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! What is the best way to save data?

Hello everyone, I want to ask what is the best way to save data. I understand that I need to use Model to save. I am kind a new in c++ programming so maybe there is a way to save data in model structs? Can someone help me?for example I want to save ...

0693W00000WL5vbQAD.png
heyo by Senior
  • 2813 Views
  • 5 replies
  • 0 kudos

STM32CubeIDE rename issue

I've been working with the cubeide and touchGFX. It seemed to be working but when I tried to import another project, the IDE gave me a message stating that, even though the new TGFX project was named something else, it was going to import it as the ...

plotting multiple line series on one graph?

I generated a touchgfx project and figured out the structures. I am able to change the chart and plot new data. What I don't understand is the generator it allows me to create multiple lines but I can't figure out a way two separate the data or add...

LTDC test routines for displaying text

I am using STM32H745BIt6 device, and wanted to write a test for testing the LCD interface using LTDC.Basic text,font and color set for text, backgound color should be displayed . Where can I get the routines which I can easily port on my custom board...

ATank.1 by Associate III
  • 1210 Views
  • 1 replies
  • 0 kudos

Resolved! TouchGFX and ClickListener Debounce/Delay

I am having trouble with the ClickListener. I am trying to debounce the click event somehow. My first instinct is to delay and then check to see if the click is still present, but I am not sure it will work with this function because it seems that th...

File .ioc not generated

Hello everyone! I created my first project on the STM32F429I using TouchGFX by following several tutorials on the Internet.I have a big problem: after setting the graphics on TouchGFX and generating the code .. when I open the project in STM32CubeIDE...

luke514 by Senior
  • 6592 Views
  • 5 replies
  • 0 kudos

Throttle position visualization

Hello,I have written my 4 bit grayscale, 256x64 OLED driver using SPI, and I want to visualize my throttle position. The throttle value ranges between -100 and +100 where -100 means maximum deceleration and +100 the maximum acceleration. So far, I ha...

0693W00000WL8TGQA1.png 0693W00000WL8TLQA1.png 0693W00000WL8TVQA1.png
fing by Associate III
  • 1138 Views
  • 0 replies
  • 1 kudos