Skip to main content
CJans.1
Associate III
November 4, 2022
Solved

DMA transfer error but CFSR does not indicate bus error

  • November 4, 2022
  • 3 replies
  • 1528 views

I'm using a STM32H743.

I used STM32CubeMx to configure the DCMI. It uses DMA to transfer to memory.

When calling HAL_DCMI_Start_DMA(), the DCMI_DMAError() function is called.

I found out that there is a transfer error. And according the documentation a bus error is the reason.

But the CFSR register of the MCU is zero, indicating no bus error.

What could be wrong?

Things I did:

  • use STM32CubeMX to set up DCMI and enable DMA
  • Disabled caching
  • created a buffer in SRAM1 using
    • __attribute__ ((section(".buffer"), used)) uint32_t bigbuf[30000];
    • checked that it is present in region RAM_D2
  • called HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_CONTINUOUS, (uint32_t)bigbuf, ((752*480)/4)/4);
    • HAL_OK is returned
    • sensor is 752*480, I use 8 bit DCMI (thus 4 in a word) and I use half the number of pixels and half the number of lines
  • checked with oscilloscope that DCMI is working (clock, sync and data signals present)

Any idea why I can get this transfer error?

This topic has been closed for replies.
Best answer by CJans.1

I found the problem! It is a bug of STM32CubeMx.

STM32CubeMx generates this code to initalize all peripherals:

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DCMI_Init();
 MX_I2C1_Init();
 MX_I2C2_Init();
 MX_UART5_Init();
 MX_USART1_UART_Init();
 MX_DMA_Init();
 MX_USB_DEVICE_Init();

The problem is that MX_DCMI_Init() initializes the DMA. But the DMA clock is not enabled yet! It is enabled by MX_DMA_Init().

I did not want to change the initialization order, so I enabled the DMA clock just before all the inits:

 /* USER CODE BEGIN SysInit */
 
 __HAL_RCC_DMA2_CLK_ENABLE();
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DCMI_Init();
 MX_I2C1_Init();
 MX_I2C2_Init();
 MX_UART5_Init();
 MX_USART1_UART_Init();
 MX_DMA_Init();
 MX_USB_DEVICE_Init();

And now it works!

3 replies

Tesla DeLorean
Guru
November 4, 2022

>>But the CFSR register of the MCU is zero, indicating no bus error.

The MCU doesn't do the DMA, or have visibility, as to what the DMA Controller is doing / using.

Look at the Bus Matrix, and how that relates to the DMA Unit, and the Memory you're acting on.

Some memories are not visible / usable. Be sure of where your buffer is situated.

Check alignment.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
CJans.1
CJans.1Author
Associate III
November 4, 2022

Thx Tesla DeLoran

I'm using SRAM1 which should be accesable by the DMA. It starts at 0x30000000.

You say 'Look at the Bus Matrix': Do you mean to find out what the bus error is? Or do you mean that I have to program the Bus Matrix? (I assumed STM32CubeMx does that).

CJans.1
CJans.1AuthorBest answer
Associate III
November 6, 2022

I found the problem! It is a bug of STM32CubeMx.

STM32CubeMx generates this code to initalize all peripherals:

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DCMI_Init();
 MX_I2C1_Init();
 MX_I2C2_Init();
 MX_UART5_Init();
 MX_USART1_UART_Init();
 MX_DMA_Init();
 MX_USB_DEVICE_Init();

The problem is that MX_DCMI_Init() initializes the DMA. But the DMA clock is not enabled yet! It is enabled by MX_DMA_Init().

I did not want to change the initialization order, so I enabled the DMA clock just before all the inits:

 /* USER CODE BEGIN SysInit */
 
 __HAL_RCC_DMA2_CLK_ENABLE();
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DCMI_Init();
 MX_I2C1_Init();
 MX_I2C2_Init();
 MX_UART5_Init();
 MX_USART1_UART_Init();
 MX_DMA_Init();
 MX_USB_DEVICE_Init();

And now it works!