STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX Slider can be set in between values

The range of the default Slider of TouchGFX can be configured by a min and max integer.When the value has changed you can get a callback with the new value as an integer.Still when moving the slider it is possible to set the location of the indicator...

EmbDev by Senior
  • 3039 Views
  • 5 replies
  • 1 kudos

Resolved! Troubleshooting White Blank Screen Issue After OCTOSPI1 GPIO Configuration in TouchGFX Application

Hi Community, I am encountering an unexpected white blank screen issue in my TouchGFX application after configuring the GPIO pins for OCTOSPI1 peripherals. The application was previously functioning correctly, but the problem arose after making chang...

Ayoub_Bnina_0-1707346182784.png

Resolved! Hard fault issue with octospi and touchgfx

Hello,I am working on a project that uses a STM32H7B3I-DK Board and an octospi memory MX25LM51245G. I also use the touchgfx library for the graphical interface.I encountered a hard fault issue that occurs randomly during the initialization of touchgf...

TouchGFX - import to STM32CUBEIDE

Hello,I have a STM32F746-DISCO development board and I use TouchGFX. When creating projects in TouchGFX and saving the project under the name APL1, this project appears in TouchGFX as APL1, but when imported into STM32CUBEIDE, it is imported as STM32...

JNova.0 by Associate III
  • 1947 Views
  • 2 replies
  • 1 kudos

Resolved! How to modify TouchGFX source files in CubeIde ?

I'm working on a STM32F469I-DISCO board. My project isn't difficult I think. I want to aquire datas with a radar and display some information on the screen in function (like distance between objects and later draw them at different places on the scre...

xth by Associate
  • 1228 Views
  • 1 replies
  • 1 kudos