STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Dynamic Page design

Hello, can you create a dynamic Page with Touchgfx? That means when the board is running, create a new widget. The widget and the number of windows are not predetermined and change while the program is running. best regard

Fereidoun by Associate II
  • 2800 Views
  • 5 replies
  • 1 kudos

Partial Frame Buffer & Slide Transition

I'm using an STM32U535 and ILI9341 touch display for my project.  I have the screen up and the touch control working with 5 screens, using forward/back buttons to navigate.  The simulator shows the slide transitions correctly but when I push it to my...

STM32F423ZHT6 support TouchGFX

Hi, I create a project with the guide of YouTube video: https://youtu.be/mU5eZ_EXW8c?si=TKkxluzNMeVRQCFG I'm using STM32F423ZHT6. Here, there is no hardware graphics accelerator like the Chrom-ART Accelerator (DMA2D) or LTDC, which are not present in...

Meenakshi by Associate III
  • 863 Views
  • 1 replies
  • 0 kudos

Resolved! Standard SPI memory without FMC and Touch GFX

Hello,i have question about external memory storage.Can be external serial memory used as a storage for Touch GFX images connected via standard SPI(MISO,MOSI, SCK and software driven NCS) to the MCU STM32F767 without FMC_NCS? Is it possible? Thanks

Petr3 by Associate III
  • 1084 Views
  • 1 replies
  • 0 kudos