STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to implement "SwitchScreen()" in touchgfx?

Hello all, I am trying to switch the screen throuch code in touchgfx.If I use SwitchScreen, how shall I state the argument (screen* newScreen)?If, for example I want to switch to Screen7. Shall I call the function with SwitchScreen(scr7)?where scr7 i...

kvkhekale by Associate II
  • 18775 Views
  • 33 replies
  • 3 kudos

Resolved! Changing from LCD16bpp to LCD8bpp

Hello, I am facing an issue where the rendered frame buffer is printed on the display as gibberish pixels.I'm using the Nucleo F746ZG and interfacing it (over SPI) with an external display controller that writes to a 240*320 display. I was not able t...

bornamm_0-1716256740120.png bornamm_1-1716257064226.png
bornamm by Associate II
  • 4970 Views
  • 9 replies
  • 1 kudos

Bug report: Wildcard use and swapping text.

Hello,I found an "edge" case with TouchGFX Designer.I have a message box that can swap syntax between language and wildcard count.think of:-ID1: "Clock stop"-ID2: "Clock <min>"-ID3: "Clock <sec>.<usec>"I was able to set a base class with id3 and both...

Marc_LM by Senior
  • 875 Views
  • 1 replies
  • 1 kudos

How to know the active screen from model.cpp

I would like to check which screen is activated from model.cppI tried to use getCurrentScreen() in touchgfx::Applicationhttps://www.touchgfx.com/documentation/html/classtouchgfx_1_1_application_af560e49a149b6d2d0ccffd4ca42e5991.html#af560e49a149b6d2d...

COSEBE by Senior
  • 4153 Views
  • 6 replies
  • 7 kudos

Resolved! Callbacks between container and view

Hi, I went through some other discussions discussing a similar problem, but they did not seem to help. I have screen one which displays (dynamically) a container. The container has a button on it, which when clicked, changes screens to screen 2. At t...

Priyank by Senior
  • 5096 Views
  • 13 replies
  • 1 kudos