STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1725 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4873 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9560 Views
  • 5 replies
  • 3 kudos

Only profiler could turn the motor

Hello,I am using the MC Workbench V6.3.1. When I generate the code and the profiler is activated, I can run the profiler and the profiler learns motor parameters and turns the motor. After that, when I go to "Motor Pilot", I can turn the motor. But w...

MP_Fault.jpg MP_AdvConf.jpg

Support for MCSDK for STM32H747XIH6

We have an application where we need to use the STM32H747XI with it's MIPI DSI display and the corresponding application running on CM7 and we need to commutate a BLDC motor on with the CM4. There is support for NUCLEOH745ZI on on the STM32CubeMX but...