User Activity

There are two motors, a large motor (Motor1)driven by discrete gate drivers and mosfets, and a small motor (Motor2)driven by the integrated driver L6230.For performance reasons, Motor1 needs a 3 sample resistor scheme (R3_2, ADC1+ADC2), so what curre...
In MCSDK 6.2.0, it says "Selected hardware boards do not support this feature". In MCSDK 6.3.2, nothing.Why?Without this, it generates MC code using systick, and if adding FreeRTOS with CubeMX, I have to merge the systick handlers for FreeRTOS and MC...
I'm using ST workbench 6.2.0 and motor Pilot V1.2.4. NUCLEO+ IHM08M1, three shunt sensor and brushless motor with encoder. When the motor is blocked, using TORQUE control-->Torque Ramp in Motor Pilot, the actual drive current I_Q_MEAS is almost zero,...
Kudos given to