STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1736 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4882 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9583 Views
  • 5 replies
  • 3 kudos

Motor Commands to preserve pre power operation?

Hello.I am running an x-nucleo-IHM03A1 with a Nucleo-F401RE and a 24BK20-30 Stepper motor.  I have FW that allows me to push a button to arm the device and then 2 other buttons that allow me to run the device using the MOV command to create upper and...

SWenn.1 by Senior III
  • 855 Views
  • 0 replies
  • 0 kudos

Resolved! HSO PI tuning with MCSDK 6.3.1

Hello, I am getting up and running with the STM32 ZeST Kit to evaluate the HSO capability. Components: 1) STEVAL-LVLP012) B-MOTOR-PMSMA13) B-G473E-ZEST1SI am currently on MDSDK 6.3.1, and Motor Pilot V1.2.11 (MC_FOC_ZEST). I was able to successfully ...

rms_st by Associate II
  • 2065 Views
  • 2 replies
  • 0 kudos

MCSDK NUCLEO-303RE

我在使用MCSDK6.3时,功率板使用我自己的板子,控制使用nucleo-303re使用FOC模式时,生成的代码可以编译通过,但是上位机显示的跟实际的不对,也无法观察ID和IQ,同时电机启动后转速会无限制的上升,斜坡这里是6步电压模式。。使用6步模式时  实测三相6路信号中,一相为全高,一相为互补PWM,一相上桥高,下桥低     

msunny_0-1729588820439.png msunny_1-1729588916952.png msunny_2-1729588974983.png msunny_0-1729589221038.png
msunny by Associate
  • 1357 Views
  • 2 replies
  • 0 kudos