STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1734 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4881 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9577 Views
  • 5 replies
  • 3 kudos

Resolved! STSPIN fault software reset

[VERSION]: MCWB v6.3.2[TOOL]: STM32CubeMX v6.13.0, STM32CubeIDE v1.11.5[BOARD]: STEVAL-PTOOL1V1[PROJECT]: STEVAL-PTOOL1V1_6S_SLWhen the external power on/off input is used to start and stop the motor, if a fault is encountered when running, the motor...

Resolved! HSO Algorithm - where to find function definitions?

Hi, I have generated code for HSO on a workbench as recommended by the release note. I need to view definitions of following functions: But not able to view the definitions of these functions. Could you please help me to open these functions? As I ne...

Rahuld_0-1749120598489.png
Rahuld by Associate III
  • 1826 Views
  • 5 replies
  • 2 kudos

STSPIN32G0 Unused Buck Outputs

I'm looking into a multi channel motor controller design centered around the STSPIN32 series MCUs.To reduce part count and layout space, I'd like to power multiple STSPIN32G0 MCUs off a single instance of the integrated 3.3V buck converter. Are there...

mgoin by Associate
  • 707 Views
  • 1 replies
  • 0 kudos

Resolved! MotorControl Workbench Issues

I have multiple issues to report with the MC Workbench (MCWB). I am using Version 6.3.2 and trying to get a dual motor BLDC setup working on custom hardware.In the .zip-file there is a minimal project required for viewing the issues and additionally ...

M_Schmidt by Associate III
  • 3872 Views
  • 5 replies
  • 3 kudos