STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1730 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4876 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9575 Views
  • 5 replies
  • 3 kudos

Motor current distorted at high speed

Hello,I am using the FOC with hall sensor (having at 15 degree mechanical accuracy) on a BLDC motor controlled by STEVAL-PTOOL4A. I am using the MCSDK v6.3.2. I activated the Overmodulation in order to drive my motor at 18500RPM. However at this spee...

AnthonyK_0-1749718553237.png AnthonyK_1-1749718596390.png AnthonyK_2-1749718637963.png AnthonyK_0-1749722001477.png
AnthonyK by Associate III
  • 553 Views
  • 0 replies
  • 0 kudos

Resolved! Drone Motor Parameters with custom board

Hello, I have made a custom board based on the EXSPIN32G4-DUAL. I want to use these motors for my project https://iflight-rc.eu/products/xing2-2207-1855kv-fpv-motor?_pos=4&_psq=XING2&_ss=e&_v=1.0.How can I get the params of the motor, is there any ch...

QuirinS by Associate III
  • 815 Views
  • 1 replies
  • 1 kudos

Connecting to STEVAL-ESC001V1

Exactly how does one connect the "Motor Profiler" to an out-of-the-box STEVAL-ESC001V1?I read all of the available documentation to no avail. Is the STLink USB hardware device required and does it need to be connected to the J4 "SWD" port?One sectio...

CSzat by Associate II
  • 9267 Views
  • 20 replies
  • 4 kudos

STMC Board Designer Clock Source - Possible Bug

I am using MCSDK 6.4.0 and am creating a new inverter board using STMC Board Designer.  I am using the STM32G474RETx MCU.When I select the Clock Source as "24 MHz External Crystal", save the project, and exit back to the list of boards, the "Clock So...

kirilian_0-1749180306070.png kirilian_1-1749180453484.png kirilian_2-1749180501801.png
kirilian by Associate
  • 826 Views
  • 1 replies
  • 0 kudos

Resolved! Motor profiler error using B-G431B-ESC1

I try to do the motor drive using a B-G431B-ESC1 board.When I connect the board, the following warning appeared.[WARNING] - MotorControlRegistersBank: Accessing register [7449] RESISTOR_OFFSET resulted in error[5] . Changing register's access accordi...

Saka by Associate II
  • 1389 Views
  • 7 replies
  • 0 kudos

STEVAL-PTOOL4A current rating

Hello,I was checking the current rating of the STEVAL-PTOOL4A. Referring to the its datasheet, it states that the maximum output RMS current is 20Amps. Howver using MC Workbench v6.3.2, it  states the maximum peak current is 34A.Which data is correct...

AnthonyK by Associate III
  • 672 Views
  • 2 replies
  • 0 kudos

Resolved! F407IGT6 Failure to use the internal clock correctly

Hello, I am currently creating an inverter using STMC Board Designer, the MCU is STM32F407IGT6,the clock source is internal clock, here are some screenshots of my configuration, it was working fine until the inverter was generated successfully, and w...

iskan_0-1749108198452.png iskan_1-1749108224752.png
iskan by Associate III
  • 735 Views
  • 1 replies
  • 1 kudos