STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1831 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4984 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9742 Views
  • 5 replies
  • 3 kudos

STEVAL-ESC001V1 example code generate failed

1. Hardware / Software setupBoard: STEVAL-ESC001V1 (MCU: STM32F303CBTx)Motor: BullRunning BR2804-1700 kVSTM32 Motor-Control SDK: 5.4.8 (C:\…\MC_SDK_5.4.8)MC Workbench: 5.4.8.21553STM32CubeMX: 5.4.0, 5.6.1, 6.4.0STM32Cube F3 FW: 1.11.3Target tool-chai...

AngHung by Associate
  • 945 Views
  • 3 replies
  • 2 kudos

3V motor control with PWM

Hi everyone, I'm currently working on a project where I'm controlling a small DC motor using a PWM signal, based on the temperature read from an LM35DZ temperature sensor. I'm using an STM32 microcontroller, and generating the PWM signal with Timer2,...

WhatsApp Image 2025-07-01 at 11.23.18.jpeg
Matija1 by Associate II
  • 1670 Views
  • 4 replies
  • 0 kudos

Resolved! power supply on evlservo1 control board

Hello,Is there a way to power the control board of the EVLSERVO1 without using the power board? I would like to just play around with the MCU before connecting to 48V for motor control. The ST-LINK V3SET does not provide any power to the board. Br,Lu...

Lukas47 by Associate II
  • 919 Views
  • 1 replies
  • 1 kudos

Micro controller required for motor control

Hi STM team,I am currently evaluating hardware solutions for a 64 kW BLDC motor control system in a VTOL (Vertical Take-Off and Landing) aerospace application. The project demands high safety assurance and performance, targeting DO-178C DAL-B or high...

Aravind R by Associate II
  • 1056 Views
  • 1 replies
  • 0 kudos

STSPIN32F0B - SIL compliance?

Dear STM Community,We are currently evaluating motor controllers for a 48V BLDC motor application and have identified the STSPIN32F0B, which features an internal gate driver, as a potential candidate.Before proceeding further, we would like to confir...

Motor wont start

Hello, I have a custom board based on the EVSPING4 Dual, the schematic is the same with the difference being no speed sensors and different mosfets. When I try to start the motor with motorpilot the speed is climbing in Motor Pilot but the motor is n...

QuirinS by Associate III
  • 1208 Views
  • 4 replies
  • 1 kudos

Motor Profiler not computing any parameter

Dear Support team,I am currently working on a NucleoF401RE and IHM07M1 driver to run a 24V PMSM motor (rated at 3600 RPM, no load).1. I am using STM32 Motor Control Workbench version 5.4.8 for motor profiling. The motor profiler doesnt compute any pa...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.