STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1743 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4892 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9594 Views
  • 5 replies
  • 3 kudos

Feature request - PWM duty cycle

Posted on October 24, 2014 at 14:38Hi Gigi, my application uses two insulated current sensors. In this configuration, STMCWB does not allow me to enter the maximum duty cycle (Control stage -> Analog inputs -> Phase current feedback -> Maximum modul...

Resolved! Need a 3rd advanced timer in the STM32 family

i would like to run 3 BLDC motors out of the STM32.  Are only TIM1 and TIM8 the only advanced timers available? is there any part that has 3? We use the comp output 3-phase PWMs with success driving 1 or 2 motors, but now we need to drive 3 and don't...

rfish.749 by Associate II
  • 1889 Views
  • 2 replies
  • 0 kudos

How to ACTUALLY get started with STEVAL-SPIN3202 ??

In order to actuate a gripper prototype, I decided to buy a BLDC motor from Maxon (EC-32 flat), and an evaluation board to drive it (STEVAL-SPIN3204, then STEVAL-SPIN3202).After setting up the hardware connection with the STEVAL-SPIN3204, I manage to...

ACAND.1 by Associate
  • 2133 Views
  • 3 replies
  • 1 kudos

How to disable MCP

Dear ST MCSDK team,We are using MC SDK 5.Y.2 and have a conflict between our custom ADCs drivers and ASPEP protocol. Aspep init the UART that use DMA and conflict with our DMA usage with ADC.We can't find anywhere to disable ASPEP / MCP Protocol in t...

ANICO.1 by Associate III
  • 3522 Views
  • 3 replies
  • 2 kudos