cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-IHM08M1 motor is running with "random" speed instead of programmed speed

Kamil Wroński
Associate III

Hi.

I'm trying to spin my motor using ST Motor Control WB and STM32CubeIDE. In my code I programmed motor speed 1500rpm, but instead of that my motor started to spin with 9000rpm speed. When I set 6500 or 9000rpm speed it spins with 1800rpm. If I try to set it using Motor Control WB or Motor Pilot is spins correctly. Can someone help me with my code in IDE?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

Dear @Kamil Wroński​ 

Welcome to the STM32 Community

Could you give more details to the STM32 Community about your setup -the material you use- ?

(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)

And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?

Best regards