Posted on February 05, 2018 at 10:55Hello, I use STSW-SPIN3202 to drive our own motor, the maximum speed is about 1800RPM(12V, 40A, max speed 2400RPM), but I use other motor driver, it can drive above to 2400RPM. When the motor's speed is above 1800...