cancel
Showing results for 
Search instead for 
Did you mean: 

Can the current controlled by the motor reach 40A? The current of the motor I see is very small and cannot meet the requirements. How can I make a 40A current motor and use it? (automatic translation)

LXU.1
Associate

Original title:

电机控制的电�?能到达40A嘛?我现在看到的电机的电�?很�?,�?能够满足�?求,我怎么能�?��?40A电�?的电机也能用呢?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Peter BENSCH
ST Employee

It may be a good idea to change the heading language to English. I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.  

Here is the translation of your question (headline) using Google translate:

Can the current controlled by the motor reach 40A? The current of the motor I see is very small and cannot meet the requirements. How can I make a 40A current motor and use it?

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Laurent Ca...
Lead II

Dear @LXU.1​ 

I changed your title "电机控制的电�?能到达40A嘛?我现在看到的电机的电�?很�?,�?能够满足�?求,我怎么能�?��?40A电�?的电机也能用呢"

by the one prposed by @Peter BENSCH​ .

Could you either confirm it is OK or edit your title if not?

Thanks by advance.

Best regards