User Activity

Hello, Sorry if this post has the wrong label/location. I have a problem with L6207 dual bridge motor driver. I am using stm32f031k6 mocrocontroller and L6207 to control two motors. While using the devices on evaluation boards they worked perfectly. ...
Hi,While I was generating a project using ST Motor Control WB v5.Y.4 encountered a problem (attachment). After generating ST Motor Control WB says "Completed with errors". Also when I try to write my own code to control my BLCD motor many vital funct...
HiI am new to FD CAN and I need to use it in my project. I have a problem with recieving data on NUCLEO-G431RB. THe data is sent by other NUCLEO-G431RB and my reciever doesn't recieve anything. My oscilloscope shows that data is correctly tranfered t...
As I wrote above I just need to learn how to write a working program to control a BLDC motor using STM32CubeIDE. It's a general question, but I do not need more. I am trying to do it by myself for months, but I have no idea how to write my code corre...
Hi.I'm trying to spin my motor using ST Motor Control WB and STM32CubeIDE. In my code I programmed motor speed 1500rpm, but instead of that my motor started to spin with 9000rpm speed. When I set 6500 or 9000rpm speed it spins with 1800rpm. If I try ...