2021-06-16 12:40 AM
I have been using the STEVAL-IDP005V1 sensor to capture data from a motor, but the sensor has stopped working.
I'm not able to retrieve it. I suspect it was a short circuit during one of the tests.
Is there any way to know if the sensor still works? any hardware check that can be done?
Thanks for your help.
2021-06-27 7:53 PM
Dear @RMedi.3
Welcome to the STM32 Community
I am not sure your question is related to STM32 Motor Control topic (mainly focuses on STM32 MC SDK tools suite)?
Whatever.
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards
2021-06-27 7:54 PM
Adding of Motor Control Hardware topic.
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.