STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1720 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4870 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9555 Views
  • 5 replies
  • 3 kudos

Max app current on MOTOR PILOT

Hello,​I am setting up a SPMSM driving system with EVSPIN32G4 and ST Motor Control Workbench.​In ST motor Control Workbench, I set the nominal current as 23 Apk.However, the max app current is determined to 10A in MOTOR PILOT.I attached screen shots ...

0693W00000KcgOLQAZ.png 0693W00000KcgOkQAJ.png
JLee.56 by Associate
  • 1631 Views
  • 2 replies
  • 1 kudos

STSPIN32F0 �?서 PIN�?� 모�?�?�서, PA14(SWD_CLK)를 특정 조건�?서 UART로 사용하였는�?�, �?�후 downlaod를 할 수 없습니다.

STSPIN32F0�?� PIN�?� 모�?�?�서, PA14(SWD_CLK)를 UART로 사용하여 log message를 보려고 구현하였습니다.그런�?� �?�후�? Download를 할 수 없어서, 문�?� 드립니다.​현재 �?� �?태�?� MCU를 다시 Download할 수 있는지요?​PIN�?� 모�?�?�서, PA14를 UART로 사용하고 다시 Download할 수 있는 방법�?�나 예제가 있으면 공유가 가능한지 문�?� 드립니다.

dkwon.1 by Associate
  • 929 Views
  • 0 replies
  • 0 kudos

Resolved! Synch TIMs on G0B1RE

Hello, I'm working with the NUCLEO-G0B1RE, controlling some motors.In order to correctly control motor I need to synchronize to timers. For this, I chose to use TIM3 and TIM15 TIM15 on Slave-Gated modeMy issue is that when the TIM3 and TIM15 start ru...

0693W00000Kc8lCQAR.png 0693W00000Kc8p3QAB.png 0693W00000Kc8o5QAB.png
Sego2 by Associate III
  • 3438 Views
  • 8 replies
  • 0 kudos