2019-09-01 5:27 PM
with stm32g431 how can detect motor parameter in ac induction motor without motor profiler only with algorithm program in side micro controller without computer software
Solved! Go to Solution.
2021-06-28 5:46 AM
Dear @omid hamdi
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
2021-06-27 9:51 PM
Adding of STM32 Motor Control topic.
Best regards.
2021-06-28 5:46 AM
Dear @omid hamdi
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards