2019-12-21 5:48 AM
i want to make 3ph inverter for induction motor speed control i cant understand how to generate 6igbt gate pulse with PWM using stm32f407 disco board timers have only 4-chanel.
Solved! Go to Solution.
2021-06-28 5:44 AM
Dear @parth kothiya
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
2020-09-10 11:54 PM
Dear parth kothiya
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-09-11 1:59 AM
yes i am facing this problem still now.
Thank you for giving attention on my question.
can you please provide any suggestion or example it is really helpful to me.
I also want to protect my firmware using encryption.
2020-09-23 8:32 AM
Dear @parth kothiya
Do you work with STM32 Motor Control SDK?
Best regards
Laurent Ca...
2020-10-16 2:06 AM
Dear @parth kothiya (Community Member)
Could you give more details to the STM32 Community about the material you use (HW and SW, CPU(s), tools and versions, board(s), motor(s) and so on)?
And more especially did you use MC tools (such as MC_suite, MC-Motor Profile, MC-SDK, MC-workbench, and so on)?
Best regards
Laurent Ca...
2020-10-26 1:28 AM
Dear @parth kothiya
As you do not answer, I guess you don't have to solve this problem anymore, therefore I consider this thread closed.
If not, feel free to reopen it by posting an answer.
Best regards
Laurent Ca...
2021-06-28 5:44 AM
Dear @parth kothiya
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards