STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1719 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4870 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9555 Views
  • 5 replies
  • 3 kudos

How can I configure the board under senseless mode?

Hello Everybody,Here are the software and boards in this case:1. MC workbench 6.3.22. STEVAL-IHM039V1/STEVAL-CTM009V1I have an I-PMSM motor, and I use the board (STEVAL-IHM039V1/STEVAL-CTM009V1) to run the ST Motor Pilot for spinning the motor. Howev...

039V1_senseless_startupFault.jpg
DF_MC by Associate III
  • 597 Views
  • 2 replies
  • 0 kudos

What is the most likely cause of the motor noise?

Hello Everybody,Here are the software and boards in this case:1. MC workbench 6.3.22.STEVAL-IHM039V1/STEVAL-CTM009V1I am using an I-PMSM motor with the ST development boards (STEVAL-IHM039V1 / STEVAL-CTM009V1). In open-loop mode, the motor spins smoo...

039V1_009V1_hall.jpg
DF_MC by Associate III
  • 632 Views
  • 3 replies
  • 0 kudos

The project does not build in "CubeIDE".

Development environmentMotor control workbench Version: 6.4.0STM32CubeMX Version: 6.16.0STM32CubeIDE Version: 2.00.0Controler/Driver: B-G431B-ESC1 kitI want to drive a 30W BLDC motor using the B-G431B-ESC1 kit.I'm currently following the instructions...

realcrew by Associate II
  • 606 Views
  • 3 replies
  • 0 kudos

Resolved! MCSDK STSPIN32g4 disable via Vcc

Hello,I'm working with a custom board that uses an external 12V supply for the VCC pin (gate driver supply) of STSPIN32g4. The VCC supply is interrupted by external circuitry whenever a fault is detected.The problem I'm encoutering is that when the 1...

Favand by Associate II
  • 637 Views
  • 4 replies
  • 1 kudos

Current Sensing

Current Sensing的这两个参数应该怎么填,该如何计算得到,或者有官方文档介绍吗?How should these two parameters for Current Sensing be filled in? How should they be calculated? Or is there any official documentation available?

Ethan_hu_0-1764573490318.png
Ethan_hu by Associate
  • 296 Views
  • 1 replies
  • 0 kudos

Why the motor start with MC_OVER_CURR error?

Hi there,I have a DIY board similar to EVSPIN32G4. Below is the three-shunt sensing circuit(In internal OpAmps, differential, external gain mode)Because the STSPING4 doesn't support internal OpAmps, differential, external gain mode, I just use the be...

Junde_0-1764138125903.png Junde_1-1764138515887.png Junde_2-1764138530032.png
Junde by Senior III
  • 746 Views
  • 2 replies
  • 0 kudos