2025-05-07 12:14 AM
Hi,
I am using a Stepper motor and the motor driver IC used is STSPIN220. I have to measure the torque of the motor to find when it has reached maximum load. What is the best way to do it?
2025-05-27 5:21 AM
Hello @Jeremiah,
the STSPIN220 cannot measure the torque of the motor.
The most effective way to measure motor torque and identify the maximum load point is by using a dynamometer.