STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9547 Views
  • 5 replies
  • 3 kudos

motor won't start with motor pilot

Okay, finally got motor pilot to come online. I was compiling code in debug mode which oddly is set to default in STM32cubeIDE. So set to release and wala, motor pilot came online. Now, I'm not getting anything from my motor. but there is this error ...

A1bucker by Associate III
  • 2142 Views
  • 1 replies
  • 1 kudos

How to run a small induction motor with STEVAL-CTM012V1

I am trying to run a small, three phase induction motor from a single phase supply. The STEVAL-CTM012V1 has more than enough power rating. I have wasted hours trying to get something working. All the files I can download seem to want to do fancy FOC ...

Dense505 by Associate II
  • 1373 Views
  • 1 replies
  • 0 kudos

STSPIN32G4 buck output dropped trigger uvlo protection

I use Internal comparator trigger Timer etr function to impelement cycle-by-cycle current mode control. I got uvlo protection when motor at heavy load(~40A pk).But when i use voltage control ,it would not occur. Does any one occur this problem?​GHSU-...

0693W00000WJaakQAD.jpg 0693W00000WJaaaQAD.jpg 0693W00000WJaaLQAT.jpg
XShiy.1 by Associate
  • 827 Views
  • 0 replies
  • 0 kudos

How to control Stepper Motor with Nucleo-L476RG

I am using the Nucleo-L476RG and I have bought a 28byj-48 Stepper motor with the ULN2003 Driver. I need to control the motor using STM32CubeIDE and am wondering how to configure a stm project to control the motor at any capacity.

JEscu.2 by Associate II
  • 2218 Views
  • 1 replies
  • 0 kudos

stm32f334 llc full bridge

hi any one can help how to got sorce code stm32f334 for full bridge i need for design 10kw sic dc to dc this power not allowing on online desin st