STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1740 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4888 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9587 Views
  • 5 replies
  • 3 kudos

How to control Stepper Motor with Nucleo-L476RG

I am using the Nucleo-L476RG and I have bought a 28byj-48 Stepper motor with the ULN2003 Driver. I need to control the motor using STM32CubeIDE and am wondering how to configure a stm project to control the motor at any capacity.

JEscu.2 by Associate II
  • 2232 Views
  • 1 replies
  • 0 kudos

stm32f334 llc full bridge

hi any one can help how to got sorce code stm32f334 for full bridge i need for design 10kw sic dc to dc this power not allowing on online desin st

FOC command is sometimes stuck

Hello, I'm controlling a BLDC motor with MCSDK 6.0.0 and IHM08M1, with FOC with 1024 PPR encoder. I compute torque (Iq_ref) commands to achieve speed control, this works ok except in rare case described below:Sometimes the MCSDK seems "stalled": I se...

E5 power supply requires hardware reset

Hi, I am using a Nucleo F401RE and a X-Nucleo-IHM07 shield for motor control applications. I am supplying 24V to the X-Nucleo via J1. I have removed jumper J9. I am then taking the 24V and dropping it to 5V and supplying it to the E5 pin. I have move...

EPaig.1 by Associate
  • 975 Views
  • 0 replies
  • 0 kudos

Resolved! STEVAL-SPIN3201 complementary PWM and dead time.

HelloI have a steval-spin3201. It includes stm32f031 mcu. I am programming it by using stm32cubeide. When I was testing PWM and dead time, I noticed that the one of phase output is not synchronous with mosfet gate signal.I shared the scopes below. Ca...

0693W00000WIGEmQAP.png 0693W00000WIGESQA5.png 0693W00000WIGE3QAP.png 0693W00000WIGEwQAP.png