User Activity

Project generation -> "UPDATE" does not update STM32 pin assignment.AN5166 2.4.3: The preferred way to change pin assignment is obviously through the STM32 MC Workbench.The only way to change pin assignment through STM32 MCSDK is to select "GENERATE"
There is only a very small movement of the motor shaft one time back and forth.I've verified right connection and correct signals from my ABZ encoder.Could this problem be linked to G4 rev Y errata issues with ADC ?
Motor Profiler and P-NUCLEO-IHM03 does not work (time out every time).GBM2804H-100T Motor Specifications:Configuration: 12N14PMax Rotation Speed: 2180Test Current: 0.0099AMax Current: 5AWhich settings for Motor Profiler works with the P-NUCLEO-IHM03 ...
ST Motor Control Worbench example reference MAGTEC motor but doesn't state type.Does anybody have suggestions for an affordable test motor to use with this kit ?PMSM15-20kW 1500-2000rpm5 polepairs560VDC (bus voltage)Encoder
Kudos given to