STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

L6474 communication works but motor is not turning

I have connected various stepper motors to multiple x-nucleo-ihm01a1 shields on a NUCLEO F466RE.The code is the same as ST's X-CUBE-SPN1 (i just changed the function names) In main() after SPI has been initiliazited at 2MHz at mode 3, I set the regis...

0693W00000WIwHTQA1.jpg 0693W00000WIwGuQAL.png 0693W00000WIwGpQAL.png 0693W00000WIwGGQA1.png
ZHama.1 by Associate II
  • 1478 Views
  • 1 replies
  • 0 kudos

STM32CUBEIDE support for STEVAL-ESC002V1?

Is there any chance that STM32CUBEIDE will have support for STEVAL-ESC002V1?If not - what is the fastest way to do development for this eval board using the IDE?Generally - as a new user of STM products, the overall impression I get is once of chaos....

ABlak.1 by Associate III
  • 6128 Views
  • 10 replies
  • 1 kudos

B-G431B-ESC1 Encoder Problem

HiI want to make a position control with a B-G431B-ESC1.I use a motor with an encoder with 1024 PPR.Motor profiler ended with no problem.I started a project in motor control workbench Ver. 5.Y.1.21203 setting the encoder in motor settings and in spee...

Gmatt.1 by Associate II
  • 5016 Views
  • 12 replies
  • 0 kudos

UM1848 Documentation needs to be updated. It is from February 2016 (DoclD027273 Rev 2) and STM32CubeIDE has changed a lot since then.

I just bought a NUCLEO-F104RE and the X-NUCLEO-IHM01A1.The main problem is have is where to put the en.x-cube-spn1 files. The instructions in Section 3.3 need to be a little clearer and more specific. Also there is no .ioc file in the software. Do yo...

0693W00000WKvCHQA1.png
KiptonM by Lead
  • 5628 Views
  • 16 replies
  • 1 kudos