STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

How do I use the Motor Pilot 6.1.0?

I have a motor running in the V1.1.3 Motor Pilot.Now what?I built a 6step controller of a hi-revving, low inductance/resistance motor. It compiled in STM32CubeIDE and is pushed to the board.I started the motor pilot and successfully connected to the ...

0693W00000Y75RRQAZ.png 0693W00000Y75RHQAZ.png 0693W00000Y75R7QAJ.png
ABlak.1 by Associate III
  • 1055 Views
  • 1 replies
  • 0 kudos

How can I allocate port D2 as the Encoder Z pulse input?

The "documentation" suggests that any IO port that can act as an interrupt is usable, but the motor control workbench only has selections for A2, A9 and B10, all of which are used for other peripherals. The document suggests selecting a "dummy" port...

jartim by Associate III
  • 1724 Views
  • 2 replies
  • 0 kudos