STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

After an upgrade to IDE 1.11.0 on the windows platform, my project would no longer build. The project...Builders list was empty.

I had IDE 1.10.1 and a Nucleo-G431RB board. We created a 6 step project using motor control Workbench, Motor Pilot and the project would build successfully. The IDE updated to Windows 1.11.0 and the project would no longer build. The builders list wa...

FTrac.1 by Associate II
  • 4073 Views
  • 12 replies
  • 0 kudos

Any Evaluation kit based on STM32G051C6 is available ?

Hi,We are planning to develop a motor driver application with stm32g051c6 micro controller. While searching, we couldn't find an EVK board with the same MCU. We have found some alternative EVK boards(NUCLEO-G031K8, NUCLEO-G070RB, NUCLEO-G071RB, NUCLE...

ASALU.1 by Associate
  • 2285 Views
  • 4 replies
  • 0 kudos

Resolved! How can we check that the compiler use ASR and not LSR?

Below is a copy of a warning found within the PID-controller of MC-SDK 5.Y.4.We have a Cortext-M4 based board so I guess the warning text is a copy-paste and I should not care that it mentions Cortex-M3.. /* WARNING: the below instruction is not M...

roar by Associate II
  • 2302 Views
  • 3 replies
  • 0 kudos

Resolved! [SOLVED] I was working with Arduino between G431rb and Sabertooth 2x32. Everything is working well but not stable. I decided to remove Arduino but couldn"t handle communication between Sabertooh 2x32 and G431rb.

I checked the signals are going to the driver from Arduino on the Hercules desktop app. I tried to send these with USART but i didn't get any response. uint8_t openRightSS[5] = {0x31, 0x32, 0x30, 0x0D, 0x0A}; // i got these hex numbers from hercules,...

cihadkck by Associate II
  • 1387 Views
  • 1 replies
  • 0 kudos