STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4882 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9582 Views
  • 5 replies
  • 3 kudos

Error coming while generating the project on MC Workbench. Using STEVAL SPIN3204 STSPIN32F0B. And at end it shows Completed with errors. Please have look-

Error: Found unsupported composite condition: CLASS='Data Exchange' GROUP='STM32_MetaDataManager'Found unsupported composite condition: GROUP='STM32_MetaDataManager' CLASS='Data Exchange'Kindly give suggestion.

YBhat.4 by Associate II
  • 1299 Views
  • 1 replies
  • 0 kudos

UM1052 Back emf waveform

In the determination of the Hall electrical phase shift shown in the UM1052 document Please tell me BemfC i am assuming it is C with respect to A ?BemfA is Phase A with respect to B?BemfB is Phase B with respect to C?I mean it is the phase to phase v...

_legacyfs_online_stmicro_images_0693W00000bl31EQAQ.png
SRedd.5 by Senior III
  • 845 Views
  • 0 replies
  • 0 kudos

Resolved! Porting Project to Pin Compatible MCU in STM32CubeIDE

I am currently working on a motor controller project with the STM32G473RE.I am trying to get more prototype boards made but the STM32G473RE is not in stock anywhere with long lead timeI see that the STM32G474RC has plenty of stock in multiple locatio...

KYin.2 by Associate II
  • 7549 Views
  • 4 replies
  • 0 kudos

Resolved! How to run a motor using ST Motor Pilot 6.1.1

similar question as https://community.st.com/s/question/0D53W00001wHk5BSAS/motor-wont-start-with-motor-pilotI am trying to run a BLDC motor using Motor Pilot 6.1.1 with B-G431B-ESC1.Here's my process.profile motor using motor profilergenerate code us...

_legacyfs_online_stmicro_images_0693W00000bkQUlQAM.png
JKong.3 by Associate III
  • 3001 Views
  • 1 replies
  • 0 kudos

My question is, is it possible view the given PWM to the GATE pin of high side MOSFET via microcontroller pin or the PWM logic is controlled by the logic circuit i.e inside of the STSPIN.

We are trying to use STSPIN32G4 Evolution board for our ventilator air blower driver application.We are facing the problem that we are receiving Speed feedback error while we connect our motor with STSPIN board via ST's Motor Driver Workbench (Motor ...

rkuma.21 by Associate III
  • 4334 Views
  • 6 replies
  • 0 kudos

Resolved! Open Loop Mode in MCSDK

I have seen the following options in the software in MCSDK  MCI_CMD_SETOPENLOOPCURRENT, /*!< set open loop current .*/ MCI_CMD_SETOPENLOOPVOLTAGE, /*!< set open loop voltage .*/in mc_interface.h file, but i don't see any source code related to them d...

SRedd.5 by Senior III
  • 8080 Views
  • 13 replies
  • 0 kudos