Skip to main content
dannypkchan
Associate III
May 1, 2022
Question

G431-ESC board FOC + HALL SENSOR spin under MCWB but not on generated codes

  • May 1, 2022
  • 0 replies
  • 634 views

My motor can spin with profiler and MCWB, it's sensored so I don't need to setup the startup parameters, then generate the source code and import into CUBEIDE, copy the MCWB generated PID Gains values, build and debug, suppose if I press the little SW1 button, it will spin, but unfortunately NOT ! 

I can use on-board's potential meter ADC as hFinalSpeed value for MC_ProgramSpeedRampMotor1() command.

I can make small I-PMSM single pole pair motor spin, however when replace with bigger motor e.g. 6 inch 6 pole pair SM-PMSM motor, I couldn't make it spin and strange thing was when I increase hFinalSpeed value, motor not start or spin  

can anyone help to point out which parameters I should focus to ?  

Hardware : G431-ESC-1 board

MCSDK : 5.4.8 (version 6 could not connect with G431-ESC with UART)

Motor : 

Pole Pairs : 6

Max. Application Speed : 1980

Nominal Current : 4.00

Nominal DC Voltage : 29.2

Rs : 0.10

Ls : 0.093

B-Emf constant : 7.8

Inertia : 91.730

Friction : 61.938

regards,

Danny

This topic has been closed for replies.