STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1749 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4901 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9613 Views
  • 5 replies
  • 3 kudos

ST MC Workbench Generation Fails

I am experiencing a "Code Generation" failure in ST Motor Control Workbench, even after performing a clean installation. I have read similar posts and did suggests.To eliminate any "Turkish character", "Path length", or "User permission" issues, I cr...

Resolved! How to connect two motors to an STM32H7 using MC Workbench

STM32H755ZITxにX-NUCLEO-IHM07M1を2個接続し、FOC制御がしたいです。MC Workbenchを使用し、STM32H7シリーズからカスタムボードを作成し設定しました。しかしソースコードを生成しようとするとエラーが発生します。この問題を解消する方法はありますか。カスタムボード、MC Workbenchのプロジェクト、生成時のエラーのスクリーンショットをアップロードします。

Tomoya66 by Associate
  • 404 Views
  • 1 replies
  • 1 kudos

Resolved! Understanding timing constraints for FOC

Hi there! Apologies if this is not the right place to be asking this question, but I'm deep in the weeds writing my own motor controller from scratch, and have a question about timing:My setup uses the STSpin233 with three-shunt low-side current sens...

sb_st by Senior II
  • 871 Views
  • 1 replies
  • 1 kudos

Resolved! Electronic gearing hardware selection

Hi - I have a new application where I'm trying to slave 1 axis to another axis. The application is an autonomous winch. The master axis drives the winch drum, the slave axis drives a level wind that makes sure the winch line is approaching the drum a...

geneM by Associate II
  • 1455 Views
  • 3 replies
  • 2 kudos

STM32G474 runaway at high RPMs

Hi, I'm struggling with a runaway situation when I try to run my motor at high RPMs. Here is my setup: 48V power supply, 300A max. The motor has 21 pole pairs. I use the FOC algorithm to drive the motor, sensor-less speed sensing (no hall sensor). I ...

Resolved! B-G431-ESC1 Electronic Speed Control PWM issues

Hello,I apologise in advance if my post lacks any important information, I am very new to working with these sorts of boards and have limited experience with motor control in general. I am using a B-G431-ESC1 to drive a 24V hoverboard motor. I have p...

rudyard by Associate III
  • 2413 Views
  • 13 replies
  • 7 kudos

Sensorless BLDC motor control with STM32F407VGTX”

Hi everyone,I am working on a custom board based on STM32F407VGTX to control a BLDC motor, and I am looking for some guidance. My goal is to implement sensorless control (FOC or 6‑step) using this MCU, and I would really appreciate any example projec...

Ash1 by Associate III
  • 607 Views
  • 1 replies
  • 0 kudos