STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1749 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4900 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9610 Views
  • 5 replies
  • 3 kudos

Resolved! STEVAL ESC001V1 PID Tuning

When i give varying PWM signal at high frequency under range, the motor sometimes produces noise and gets stuck (0 speed even though pwm signal is valid). What is the issue? I feel its due to PID tuning. Kindly share PID tuning method.Thanks 

Resolved! FOC Control with STM32G491KE

Hi, I'm a circuit engineer in korea.I want to make really small BLDC FOC controller with STM32G491KE, because It has the smallest pin counts compare to other G491 family.For FOC Control, I have to use three TIM channel. For use external ociliator, I ...

yeseung_0-1767350262868.png
yeseung by Associate
  • 885 Views
  • 4 replies
  • 0 kudos

How to add inverter board in MCSDK6?

Hi there,My team has designed a dual motor control board, and I'm responsible for spinning the motors.I have already added the board to MCSDK6 and generated the project without error.However, when I add the code like MC_StartMotor1() after initializa...

Junde by Senior III
  • 347 Views
  • 4 replies
  • 1 kudos

Resolved! How to drive a motor with both encoder and hall?

Hi there,I have a motor support both encoder signals(ABZ) and hall signals(ABC) output.But I checked the DEV Kit and the examples of MCSDK6. Most examples use only one of the position feedback sensors.And for the MCSDK6 project, I can only configure ...

Junde by Senior III
  • 816 Views
  • 4 replies
  • 1 kudos

IHM03A1 and ARDUINO UNO Q

Powerstep01 has a beautiful function to zero the position of the counter that works in conjunction of an external switch SW. It sets the slowest speed and direction of a movement automatically and waits until a rising edge is detected on from the swi...

kafkaesq by Associate
  • 473 Views
  • 4 replies
  • 0 kudos

AC induction Motor for New Project

Hello;I want to create  Ac induction motor project. So I cannot find ACIM GUI or ACIM profile in MC Workbench any versions. Could you please give an answer for my questions1. Can i download ACIM GUI ?2. Can i find a acim profile  for mc workbench 3. ...