STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1743 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4892 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9594 Views
  • 5 replies
  • 3 kudos

PWM complementary Output

Hi,I try to implemend sinus algorithm for BLDC engine on  STM32G474RE chip.  I want to use TIM1 (CH1 - CH3) and (CH1N - CH3N) to control a bldc controller. I have configured a complementary output with dead time according to datasheat (so I think) an...

Screenshot from 2023-07-06 14-59-22.png Screenshot from 2023-07-06 14-59-31.png
Arek by Associate
  • 1164 Views
  • 0 replies
  • 0 kudos

Resolved! Hall Sensor - ST MC WB

I successfully ran the BLDC hub motor with sensorless method (sensorless + PLL) with EVSPIN32G4 hardware. My motor have the inbuilt hall sensor with 60 degree placement. Now, I am trying to configure with hall sensor. I get the speed feedback error i...

prasanthkumar22_1-1688561632862.jpeg prasanthkumar22_2-1688561937296.jpeg

Resolved! X-NUCLEO-IHM01A1 and development board

Hi STM,I am having NUCLEO-476RG and I am planning project with steppers (by using X-NUCLEO-IHM01A1). Can I connect this expansion with my development board. And also, what is the maximum number of expansion boards I can connect to the development boa...

akara.31 by Associate
  • 1656 Views
  • 2 replies
  • 0 kudos

Resolved! Motor does not start with B-G431B-ESC1 board.

Hi all,I'm new to the STM32 world and ST motor control tools, so I might be missing something obvious.I have the B-G431B-ESC1 development board connected to a BLDC motor.I generated the code for FOC with the MC-WB 6.1.2 and STCubeMX 6.8.1. Compiled w...

_legacyfs_online_stmicro_images_0693W00000blAX7QAM.png