cancel
Showing results for 
Search instead for 
Did you mean: 

How can I generate an Induction Motor Control setup through MCSDK?

Dane._.T
Associate II

Unfortunately, I cannot get MCSDK to generate the Middleware with the Induction option, as it either does not appear (v. 6.0.0) or it fails to generate pwm_curr_fdbk.c properly (v. 5.Y.4). The other two algorithms generate fine and can run my setups. From what I've seen so far, Induction seems to be newer and is only supported in 5.Y.x.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0