STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4881 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9581 Views
  • 5 replies
  • 3 kudos

How do I flash firmware to the B-G431B-ESC1?

I'm trying to get the basic firmware running, but I think I'm doing something wrong because the ESC doesn't seem to function. I've generated an IDE project for the B-G431B-ESC1 using the ST Motor Control Workbench, which I then opened in STM32CubeIDE...

ZRoma.1 by Associate
  • 3992 Views
  • 1 replies
  • 0 kudos

MCSDK 5.4.8 g++ compile problem

I don't know where to report it. In the file MotorControl/MCSDK/MCLib/Any/Inc/hall_speed_pos_fdbk.hIn Line 232 is missing:...#ifdef __cplusplus}#endif /* __cpluplus */....#endif /*__HALL_SPEEDNPOSFDBK_H*/

JRyba.2 by Associate
  • 1114 Views
  • 1 replies
  • 0 kudos

Resolved! need a 5kW motor driver board

Hi all,       I'm Siva, and i need a BLDC motor driver to run a 5kW motor. please suggest me in buying out the right driver board. the voltage needed for the motor is 48 volt and the current needed will be 180A.   

Resolved! Motor not working as expected

I'm trying to make run a motor via Motor Pilot but it does not work correctly. I'm using the following motor: 1 stücke Mitoot 5008 335KV/400KV Bürstenlosen Motor Für 1555 1755 Propeller Quad kit RC Multicopter Hexacopter Tarot T960 t810|Teile & Zubeh...

GJamo1_1-1687706903988.png GJamo1_0-1687706565796.png
GJamo.1 by Associate II
  • 1600 Views
  • 1 replies
  • 0 kudos

Resolved! No FreeRTOS for 6-step with kit P-NUCLEO-IHM03?

Hi there,I am new to motor control and I am trying to set up my P-Nucleo-IHM03 kit with MC Workbench 6.1.2. I would like to use FreeRTOS in combination with the 6-step algorithm but in the "Application Configuration" under "FreeRTOS" it is stated: "S...

Getting error: stm32g4xx_ll_opamp.h: No such file

After following all procedure I am able to generate code, But with some errors. After Loading IOC file in CubeIDE. during build I am Getting this error: stm32g4xx_ll_opamp.h: No such file.MC SDK V 6CubeIDE LatestSelected existing example of B-G431-ES...

Resolved! Can I use NUCLEO-G491RE with MCSDK6.1.2?

Hello.I want to use NUCLEO-G491RE with MCSDK6.1.2. However, NUCLEO-G491RE does not exist in the list of "Control" of MCSDK. If I have a NUCLEO-G491RE JSON file, can I import it? Where can I get the JSON file?Thank you.

Takano by Associate
  • 1391 Views
  • 2 replies
  • 0 kudos