cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G4B1C3

james farrant
Associate III

Hello,

I am trying to get my STM32G4B1C3 ESC working for a brushless rc hobbyist motor with unknown motor parameters. I flashed a generic set of parameters to the device and enabled the motor profiler before flashing so that I could estimate them online. 

 

When I connect to the motor pilot app Everything is detected fine with no faults, but then I click begin profiler and it seems to just stall with a high pitch noise and never gets past 7% complete. I have tried swapping the 3 phases in all combinations with no change in behavior:

 

Motor details:

Aerosky MC2212-980KV 

7 pole pairs with standard surface magnets (outboard)

 

1 REPLY 1
GMA
ST Employee

Hello @james farrant,

The A2212 motor is available from MCSDK6.3.1 delivery.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA