STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4882 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9582 Views
  • 5 replies
  • 3 kudos

MCSDK 6.2 and IHM042-V1 Dual Motor Position Control

Version:  MCSDK 5.4.8 / MCSDK 6.2.0Tool: Firmware / MC WBEvaluation Board: IHM042-V1Details:When using MCSDK 5.4.8 I am unable to have the first motor perform in the same manner as the 2nd motor despite all parameters being identical and the same mot...

95Z_0-1696419881195.png
95Z by Associate
  • 1713 Views
  • 2 replies
  • 0 kudos

Resolved! Some confusion about MCSDK 6.2.0

[VERSION]: 6.2.0[TOOL]: ST Motor Pilot/ MotorControl Workbench 6.2.0[DETAILS]:1.The speed ki ‘s numerical values ​​do not correspond.It is different from 5.Y.4.2. About the Board Maneger. I want to add my own board but no documentation guidance.3. Ab...

企业微信截图_16968470027075.png
gtop.1 by Associate III
  • 3237 Views
  • 4 replies
  • 0 kudos

Resolved! How can I stop the motor urgently?

Hello.I am testing using MCSDK 6.2.0 on EVSPIN32G4 board.I've checked the operation of the motor using the start/stop button.The problem takes approximately 3 seconds or more to stop during operation at a maximum speed of 16000 rpm.I want to stop urg...

Elliot95 by Associate II
  • 3181 Views
  • 3 replies
  • 2 kudos

Resolved! Rotor position intermittent missing

I have generated the code with workbench 6.1.2 planning to migrate to 6.2.0 but meanwhile i am finding one issue consistently. I am using digital hall sensors and i am constantly getting a gap as below in the rotor angle after every some duration. Is...

SRedd5_0-1696586362777.png SRedd5_1-1696586503875.png
SRedd.5 by Senior III
  • 2743 Views
  • 5 replies
  • 0 kudos

Resolved! pmsm motor control boards

Looking for a motor control board for test and evaluation of low voltage hub motors 48-80Vdc and 50-100A or at least something in tens of Amperes range; I have found that Matlab/Simulink suggests a combination of Nucleo-G474re Board X-NUCLEO-IHM07M1...

rondik by Associate
  • 2657 Views
  • 3 replies
  • 0 kudos