STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1601 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4754 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9471 Views
  • 5 replies
  • 3 kudos

Resolved! Rotor position intermittent missing

I have generated the code with workbench 6.1.2 planning to migrate to 6.2.0 but meanwhile i am finding one issue consistently. I am using digital hall sensors and i am constantly getting a gap as below in the rotor angle after every some duration. Is...

SRedd5_0-1696586362777.png SRedd5_1-1696586503875.png
SRedd.5 by Senior III
  • 2618 Views
  • 5 replies
  • 0 kudos

Resolved! pmsm motor control boards

Looking for a motor control board for test and evaluation of low voltage hub motors 48-80Vdc and 50-100A or at least something in tens of Amperes range; I have found that Matlab/Simulink suggests a combination of Nucleo-G474re Board X-NUCLEO-IHM07M1...

rondik by Associate
  • 2556 Views
  • 3 replies
  • 0 kudos

Start up motor in STC_SPEED_MODE issue

Hello everyoneI'm trying to control a motor using STC_SPEED_MODE. There's a problem at startup: I program a ramp (for example i would like to obtain 6000RPM), motor start to rotate and accelerate, but speed reach maximum speed for the motor (for exam...

Resolved! If Motor Profiler will open source?

I often use Motor Profiler to identify motors.But it is not good.Sometimes my motor cannot be recognized when using 48V and I have to reduce the supply voltage to 36V.Here I would like to ask whether it will be open sourced. I want to understand the ...

gtop.1 by Associate III
  • 3133 Views
  • 7 replies
  • 0 kudos

Resolved! EVSPIN32F02Q1S1 Fail note when connected to PC

Hello, I recently purchased EVSPIN32F02Q1S1 and attempted to flash it with the FOC firmware generated through MotorControl Workbench 6.1.2. However, I was unable to upload the code onto the board and instead greeted with the following message in Cube...

kenni_0-1696718159051.png kenni_2-1696718619208.png
kenni by Associate II
  • 1397 Views
  • 1 replies
  • 1 kudos